CodeWarrior for PPC connection problem with PowerTAP II

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CodeWarrior for PPC connection problem with PowerTAP II

3,111件の閲覧回数
MGotcha
Contributor I
I am attempting to use CodeWarrior v8.5 (for PPC) with a PowerTAP II (for the MPC824X). Host is XP w/up to date patches. I created project code using CW and can run & debug using the MWX-ICE v4.5.1 debugger software that came with the PowerTAP, but cannect get CW to connect to the powerTAP to allow debugging from CW. It finds the PowerTAP and starts communications (PowerTap TX/RX lights start flashing), but then an error appears:

CSSProtocolPlugin:
Could not connect to the probe
(Download invald length)

There is not a lot of details in the manuals on setting up the PowerTAP, and it works fine with the MWX-ICE. Suggestions? Thanks!
ラベル(1)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,524件の閲覧回数
CrasyCat
Specialist III
Hello
 
As far as I know CodeWarrior v8.5 (for PPC) supports only connection through USBTap & EthernetTAP (or PowerTAP Pro) cable.
PowerTAP II is not supported any more. So you will have to purchase a new HTI to be able to connect to your board.
 
 
CrasyCat
0 件の賞賛
返信

1,524件の閲覧回数
MGotcha
Contributor I
That's not good news! No support for hardware that's not even 5 yr old! The low cost of the USBTAP may make this not so bad. What differences are there between the PowerTAP II / PowerTAP PRO vs the USBTAP other that the obvious flexability of an ethernet interface and the COM port (neither a big deal for us). Stability and debug features are most important. Thanks again!
0 件の賞賛
返信