CodeWarrior for LS1012A

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CodeWarrior for LS1012A

3,164件の閲覧回数
artsiomstaliaro
Contributor IV

Hi,

im going to work with FRDM LS1012A board with CodeWarrior. I just downloaded last version from NXP web site (11.2.0), version for Linux. 

I do not see LS1012A in a list of supported devices. I just checked forum and seems i need to update CW.

I tried Help->Install new software with several options:

ARMv8 Eclipse Update Site - (http://freescale.com/lgfiles/updates ...)

http://cache.nxp.com/lgfiles/updates ...

But no luck. Cache.nxp.com reports - Cannot perform operation. Computing alternate solutions - then process stops.

Does anybody knows correct links i can use in CW?

Thank you.

ラベル(1)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

2,936件の閲覧回数
Pavel
NXP Employee
NXP Employee

Use the following for adding the FRDM-LS1012A supporting to CW_CW4NET_v2018.01:

Help

                Check for Update

 

See attached snapshot.

Have a great day,
Pavel Chubakov

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,936件の閲覧回数
artsiomstaliaro
Contributor IV

Dear Pavel,

unfortunately isn't working at all.

What i did:

1. I went to

NXPSoftware & Support -> CodeWarrior Development Suite Specialist Networked Evaluation -> CodeWarrior for QorIQ LS Series ARMv8 ISA. Evaluation / Updates : Files

2. Found only Installer: CodeWarrior Networked Applications Linux Hosted-Offline

          2.6 GB, CodeWarrior Networked Applications Linux Hosted-Offline v2016.01.tar

3. Installed it.

4. When i run CW 2016.01, checking for updates -> returns error (Cannot perform operation).

0 件の賞賛
返信