CodeWarrior cw_dbg.flt.elf2flt error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

CodeWarrior cw_dbg.flt.elf2flt error

2,395 次查看
jarjarbin
Contributor I
Hi,

I'm a newbie, if anyone has an answer, I would appreciate. I have used the linux stationnery wizard to create a simple soft for coldfire device. When I try to compile the project, I get the following error:

link error /usr/local/m68k-elf/bin/ld.real : can not open /test/cw_dbg.flt.elf2flt no file or folder
link error   ld return 1 exit status

thx!

标签 (1)
标记 (1)
0 项奖励
回复
1 回复

978 次查看
Alban
Senior Contributor II
Hello,

You provide too little information.
Please read the post: [IMPORTANT] When Asking about CODEWARRIOR !!!

We need the targetted MCU to figure in the subject line.
Finally, the subject line is required to mean something.

Thank you,
Alban.


Message Edited by Alban on 2007-06-27 03:13 PM
0 项奖励
回复