CodeWarior 6.2 & USB-ML-CF

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CodeWarior 6.2 & USB-ML-CF

2,025件の閲覧回数
beginneruser
Contributor I

I am using  Development Board M5213EVB and external debugger USB-ML-CF (vendor P&E Microcontroller Systems). I have a problem while loading sample  program code to the target controller. I have performed the following steps:

 

1. Installed CodeWarior (version 6.2,build 11) , included to KIT.

2. Compiled the sample project “M5213EVB CONSOLE-SRAM” from catalog (CodeWarrior_Examples)\M5213EVB.

3. Pressed button [ |> ] to debug the program. CodeWarior began to load the program to target controller, but loading process broke with the error message “ PEMicro Protocol Plugin: An Error occurred while trying to write memory” or error message “ Could not set PC to entry point”

 

What I have to do to solve this problem?

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

823件の閲覧回数
CrasyCat
Specialist III
Hello
 
Looks like there is something broken in the project.
 
I can only make following recommendation:
  1- Give it a try with the latest release of CodeWarrior for Coldfire V6.4.
      This version is available for download from our Web site.
  2- Submit a Service Request and contact our support team around that.
       Click here to submit a service request.

Make sure to attach a reproducible project and installed product information to the service request.
CrasyCat
0 件の賞賛
返信