Cannot disassemble ELF - IDE hangs

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Cannot disassemble ELF - IDE hangs

2,576件の閲覧回数
Haiiro
Contributor I
I'm using CW 6.4, P&E Multilink USB-ML-CF, Rev. C. Target is MCF5235, external flash.

I have the system working in RAM via the debugger, and I am working on making it run in flash. I can generate code that runs for a while in flash, but it eventually crashes. I am trying to track down if some memory segments are not being handled properly.

I am making use of the .xMAP files to track down how each of the segments behave. I would like to also look at the disassembly of the .ELF files, however, when I try to disassemble them the system never completes. If I try to stop the disassembly process, the IDE gets stuck at 50% processor usage and hangs. I need to use the Program Manager to stop the entire IDE.

In previous iterations of the .LCF I was able to get a disassembly listing.

Are there any known issues or tricks about this kind of problem?

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,047件の閲覧回数
CompilerGuru
NXP Employee
NXP Employee
That does not sound to good, I would suggest to file a service request. If possible attach the problematic elf file.
You can use any other decoding tool, for example gnu binutils or the decoder.exe in the CW for HC08/HC12 in the mean time.

Daniel
0 件の賞賛
返信