Can the New Project Wizard directly create a 'library' Project Type?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can the New Project Wizard directly create a 'library' Project Type?

2,582件の閲覧回数
gmnelson
Contributor III

I'm using the latest version of CodeWarrior for Coldfire (ver 7.1.1a build 9, IDE ver 5.9) and I'm trying to create a 'library' project type.  Rather than start from scratch, I'm trying to use the New Project Wizard facility to create this library.  Unfortunately, with this wizard it doesn't give me the option to specify a 'libary' Project Type.  Is this correct?  Am I missing something here?

 

Also, as I'm reading through the documentation for CodeWarrior, there is mention of a "Makefile Importer Wizard".   Unfortunately, I can't seem to find this function within CodeWarrior for Coldfire.

ラベル(1)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,604件の閲覧回数
CompilerGuru
NXP Employee
NXP Employee

I don't think the wizard offers to create static libraries.

Also there is not much in common in between different static libraries, I don't think a wizard would help much except maybe setting up the compiler search paths. For thouse I would copy them from a

wizard generated project. Note that the search paths can be copy pasted or even dragged from one project too another.

 

Daniel

 

0 件の賞賛
返信

1,604件の閲覧回数
gmnelson
Contributor III

Okay, thanks for the suggestion.

 

Yes, I was actually thinking to just create a Wizard generated 'application' project as close as possible to the static library, and then just change the settings to have the project generate a static library instead of the application.

 

 

0 件の賞賛
返信