CW8.1 PPC - Starting a CodeWarrior Project for CME555

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CW8.1 PPC - Starting a CodeWarrior Project for CME555

2,660件の閲覧回数
Andrei1221
Contributor I
Hi Everyone


This is a very beginner question, I've recently got my CME-0555 from Axiom and I would like to start a project in CW 5.5 (full version). I am reading the instructions that are provided with the board in concerns to starting such a project however I am a little confused.

The instructions go as follows
1. "Select File/New"
2. Select PowerPC EABI Stationery, type a project name, type a directory for this project and click OK.


My problem is that nowhere in CW does it say that anything about "PowerPC EABI Stationery" when I go to File->New. The choices which I see are "Empty Project", "EPPC New Project Wizard" and "Makefile Importer Wizard".

How do I get out of this problem to create a project for the Axiom CME-0555 target?

Thank you

--
Alban Edit: CW version in Subject line.

Message Edited by Alban on 2007-03-25 11:44 AM

ラベル(1)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,413件の閲覧回数
CrasyCat
Specialist III
Hello
 
Try to select "EPPC New Project Wizard" and then follow the instruction on the screen.
Please note that current version of the MPC5xx tools is V8.7 and the Quick Start there is speaking about using the wizard to create your project.
 
You may want to start with the latest release of the tools.
 
CrasyCat
0 件の賞賛
返信

1,413件の閲覧回数
Andrei1221
Contributor I
Sorry for the double post, the IDE is 5.5 but the CodeWarrior version is 8.1.
0 件の賞賛
返信