CW7.0 Pro: MCF52223: Error: "declaration specifier conflict; illegal 'bool' sequence"

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CW7.0 Pro: MCF52223: Error: "declaration specifier conflict; illegal 'bool' sequence"

2,291 Views
nbonwit
Contributor I

Hello,

Every time I make my project, I get the error "declaration specifier conflict; illegal 'bool' sequence" on the following line in PE_Types.h (which I'm assuming is an autogenerated file from Processor Expert).

/* PE types definition */
typedef unsigned char           bool;

I can't disable bool support in the C++ langauge options because I'm using booleans in my own code.  I'm assuming the error is because the PE_Types.h fils is trying to give the name 'bool' to a variable but it's already a reserved keyword (bool).  If I comment out that line, the compiler error goes away, but if I restart Codewarrior and remake the project, the error reappears (I'm assuming because it's regenerating the file PE_Types.h)

What should I do?  Any help would be appreciated.

Thanks,
Neville

Labels (1)
0 Kudos
Reply
1 Reply

1,075 Views
ProcessorExpert
Senior Contributor III
We are sorry but Processor Expert doesn´t support C++.

Processor Expert Support Team
www.processorexpert.com
0 Kudos
Reply