CW Special Edition limits

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CW Special Edition limits

2,393件の閲覧回数
nspon
Contributor II
I'm using the Special Edition of CW for Coldfire 6.2 that came with my MCF5208EVB. I understand its limited to 128K of code, but are there other limitations? I don't seem to be able to link a library that I have created to my project, although the MSL and runtime libraries link just fine, even after I rebuild them. I also don't seem to be able to add subprojects (e.g the MSL project) to my project. Are these limits of the Special Edition, or does it mean I have something wrong somewhere?

Thanks,
Nigel
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,094件の閲覧回数
CrasyCat
Specialist III

Hello

Just take a look at the document at following URL:

http://www.freescale.com/files/soft_dev_tools/doc/data_sheet/950-00011.pdf

Page 2 provides a table showing which are the limitation of Special edition for Coldfire.

I hope this helps.

CrasyCat

0 件の賞賛
返信