rs08 debugger connection lost

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

rs08 debugger connection lost

1,964 Views
ivanpotter
Contributor I

using RS08LA8 in debug mode. Debug settings are default with Debug session type as Download, .abs flash file selected usb multilink connection. No breakpoints. After debug is selected and downloaded, console message is (connection lost) - any advice ?

0 Kudos
Reply
3 Replies

1,846 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Ivan

What's your CW version? What's your windows platform? 64bit win10?

Best Regards

Jun Zhang

 

0 Kudos
Reply

1,846 Views
ivanpotter
Contributor I

CW 11.01 Build 180609 Win10 64 Bit. Using USB3 port connected to a USB2 port extender with PnE Multilink Universal.

Project builds and runs. When I right click on project and "Debug as Codewarrior", I am prompted to toggle device power -  I do that and select OK. "target connection lost". Your assistance is apreciated

0 Kudos
Reply

1,846 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Ivan

CW 11.01can support 64bit win10 without problem.

I just you check the basic connection first. Create a NEW project with wizard in a NEW workspace.Can it be downloaded?

If still has problem, install P&E latest driver:

http://www.pemicro.com/downloads/download_file.cfm?download_id=53 

then restart computer to test again.

I also suggest you test your board on another computer to verify if the problem is on board itself.


Have a great day,
Jun Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply