remove file properties

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

remove file properties

1,954 Views
asmith
Contributor III

How do I remove properties (such as optimization settings) set for a specific file so that it reverts back to using those for the folder or project ?

Labels (1)
0 Kudos
Reply
2 Replies

1,837 Views
trytohelp
NXP Employee
NXP Employee

Hi David,

The configuration can be linked to the project (all files included), folder or specific to a file.

If the properties is opened when the project is selected you will open the Project Properties.

If the properties is opened when a file is selected, you will open the file properties.

The File properties is applied on file only whereas the project properties is applied on all files included in the project.

If you open the file properties and click on "Restore Defaults" the options defined in the project properties will be applied.

If you've a specific Folder properties (different to project) when "Restore Defaults" is applied on file the options defined in the project are used.

Hope this will answer your question


Have a great day,
Pascal
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,837 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello David,

Do you use CodeWarrior ? Which version ? And about which chip ?

BR

Alice

0 Kudos
Reply