"mpc563.h" Module Code

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

"mpc563.h" Module Code

ソリューションへジャンプ
2,190件の閲覧回数
scottluplow
Contributor I


Other than the standard core manual(MPC563RM), is there a resource that explains how to use the structs (i.e. Module QSMCM) within 563.h?  The manual does not contain actual example code for using the structs (i.e. QSMCM.SPCR.R=0xa10a;  /*Master, TTL, 8bit, etc.)

 

I am new to lower level code like this and I am assuming there is possibly a supplemental guide for these structs.

 

Any help would be greatly appreciated.

 

Thank you,

 

Scott

ラベル(1)
1 解決策
2,034件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

Hello Scott

The attached file <samp563.c > contains the sample code for how to use the structures defined in head file.

It is similar for QSMCM, the code should be like:

QSMCM_A.SPCR0.R = 0xa10a

The address for QSMCM_A is defined in <mpc563.h>. Its structure type is defined in m_qsmcm.h.

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

2 返答(返信)
2,035件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

Hello Scott

The attached file <samp563.c > contains the sample code for how to use the structures defined in head file.

It is similar for QSMCM, the code should be like:

QSMCM_A.SPCR0.R = 0xa10a

The address for QSMCM_A is defined in <mpc563.h>. Its structure type is defined in m_qsmcm.h.

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

2,034件の閲覧回数
scottluplow
Contributor I

Thank you for your help!  The sample code file really helped to clarify.

Scott

0 件の賞賛
返信