integrate OSEK turbo OS08  into Codewarrior Studio HC08

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

integrate OSEK turbo OS08  into Codewarrior Studio HC08

跳至解决方案
2,758 次查看
sudi01
Contributor I
I installed Codewarrior Development Studio HC08 with peramanent license with out any problem or error messages and also installed OSEK turbo OS  HC08 and OSEK builder successfully. After installation, I should get OSEK turbo stationery in project window of Codewarrior,but Iam not getting. In OSEK builer, Iam not able to create oil file and it is showing some errors .Please find snapshot of error as attachment.
 

 

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,642 次查看
J2MEJediMaster
Specialist I
I'm using the HC(S)12 version of OSEK, but I'm hoping there's enough parallels between that and HC08 to help you out. Did you install Codewarrior first, then OSEK? Codewarrior needs to be in place first for the OSEK installer to recognize it and adopt its paths and directories. When you ran the OSEK installer, did you choose the Codewarrior integration option? This is necessary because for Codewarrior to work with OSEK, a lot of key OSEK files have to be copied into the Codewarrior directory. You can verify this by searching the Codewarrior directory for an OSEK sub-directory. Finally, OSEK projects don't show up in the project stationary choices. You have to use the New Project wizard, where you'll get prompted to use OSEK in your project. HTH.

---Tom

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,643 次查看
J2MEJediMaster
Specialist I
I'm using the HC(S)12 version of OSEK, but I'm hoping there's enough parallels between that and HC08 to help you out. Did you install Codewarrior first, then OSEK? Codewarrior needs to be in place first for the OSEK installer to recognize it and adopt its paths and directories. When you ran the OSEK installer, did you choose the Codewarrior integration option? This is necessary because for Codewarrior to work with OSEK, a lot of key OSEK files have to be copied into the Codewarrior directory. You can verify this by searching the Codewarrior directory for an OSEK sub-directory. Finally, OSEK projects don't show up in the project stationary choices. You have to use the New Project wizard, where you'll get prompted to use OSEK in your project. HTH.

---Tom
0 项奖励
回复