importing a codebench project

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

importing a codebench project

1,037 Views
toddkiefer
Contributor II

We've been using CodeBench (currently owned by MentorGraphics, formerly Sourcery) to create/edit software for a ColdFire MCF52259 processor.  The CodeBench IDE uses Eclipse.

We are no longer able to use this software on some of our systems.

I have downloaded an evaluation copy of version 10.7 of CodeWarrior (which also uses Eclipse) and it seems to work properly with the hardware.

The problem that I have encountered is that I cannot successfully import the CodeBench generated project into CodeWarrior.  Is there any way to do this so that the target processor, compiler, linker, other settings from the CodeBench project are maintained in the new CodeWarrior project?

Labels (1)
0 Kudos
Reply
0 Replies