cw 10.6 & usb mass storage device host bootloader

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

cw 10.6 & usb mass storage device host bootloader

1,563件の閲覧回数
mruetti
Contributor III

Hi

Did anyone build the AN4368 bootloader with CW 10.6?

Mario

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 返信

1,376件の閲覧回数
mruetti
Contributor III

OK, if found a newer version "USB_MSD_Host_bootloader_rev2.zip" (https://community.freescale.com/thread/103038). After importing and changeing the variable project_loc to uppercase (PROJECT_LOC) in the include path, I was able to compile the source. Unfortunately I dont have the hardware at hand, so I have to wait untli monday to check.

0 件の賞賛
返信