codewarrior 2.1 will work on windows10?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

codewarrior 2.1 will work on windows10?

4,285 Views
LINMU
Contributor I
 
0 Kudos
Reply
6 Replies

4,253 Views
LINMU
Contributor I

The processor is MPC5607B, codewarrior version is shown in the picture.I cannot open a MPC5607B project with .mcp extension using codewarrior 2.1 version.1692171860073.png

0 Kudos
Reply

4,244 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi @LINMU 

CW2.1 only supports below platforms:

  • Host platforms:
    • Microsoft® Windows® XP 32- and 64-bit (Professional Edition)
    • Vista® 32- and 64-bit (Business)
    • Vista 32-bit (Home Premium)
    • Microsoft Windows 7 32- and 64-bit (Professional Edition/Home Premium)

It doesn't support win10. If you work on win10, please use CW11.1 instead. it supports MPC5607B as well. For more about CW11.1, see below:

https://www.nxp.com/design/software/development-software/codewarrior-development-tools/codewarrior-l...

Have a nice day,

Jun Zhang

0 Kudos
Reply

4,238 Views
LINMU
Contributor I

Does CW11.1  open  .mcp project?

0 Kudos
Reply

4,199 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi LINMU ,

No. CW11.1 is based on eclipse platform. It can not open .mcp file.

User needs to port CW2.1 project to CW11.1 manually.

The suggested method is: Create a new CW11.1 project, drag the source file to the project one by one.

Hope this helps,

Jun Zhang

0 Kudos
Reply

4,111 Views
LINMU
Contributor I

Thanks!

0 Kudos
Reply

4,275 Views
Irene
NXP Pro Support
NXP Pro Support

Which processor are you using?  Can you give me information about the actual codewarrior version you are using?

0 Kudos
Reply