When I installed codewarrior V10.6 in windows XP, error"Failed to create Java virtuan machine" occurred.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

When I installed codewarrior V10.6 in windows XP, error"Failed to create Java virtuan machine" occurred.

2,514 Views
zhouzhuoqiang
Contributor I

When I installed codewarrior for MCU V10.6 in windows XP, during installing process, error "Failed to create Java virtual machine" occurred. How to solve it?

 

 

Thanks a lot!

Labels (1)
0 Kudos
Reply
5 Replies

2,262 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi,

normally this is because of the low computer memory.

is this problem happened during inatall halfway or after installation?

How about your computer system hardware configuration?


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,262 Views
zhouzhuoqiang
Contributor I

3.32GHz, 504M RAM

0 Kudos
Reply

2,262 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi,

CW10.6 needs at least 2GB RAM. 504M is not enough. see CW system requirement:

pastedImage_0.png

can this help you?


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,262 Views
zhouzhuoqiang
Contributor I

Thanks a lot!

0 Kudos
Reply

2,262 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

you are welcome!


Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply