What is .common section in map file?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What is .common section in map file?

ソリューションへジャンプ
13,344件の閲覧回数
ThomasH
Contributor II
Hi
 
I´m new in using  the CodeWarrior (4.5) for HCS12 annd I found a .common section in the map file. It seems that there are linked global variables. But I´m not sure and I can´t find a description in the docu.
 
Thanks!
Thomas
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
7,318件の閲覧回数
CrasyCat
Specialist III

Hello

Here are the predefined section used by the compiler is using:

.text : Contains the code.
.data : Contains the initialized global variables.
e.g. int a = 1, b= 2;
.stack: Contains the stack.
.bss : Contains the static un-initialized global variables.
e.g. static int c, d ;
.common: Contains the un-initialized global variables (not static).
e.g. int e, f;
.rodata : Contains the constant variables .
e.g. const int c1=2, c2=4 ;
.rodata1: Contains all the string constants.
e.g. #define mystr = “Hello world”

I hope this helps.

CrasyCat

元の投稿で解決策を見る

0 件の賞賛
返信
9 返答(返信)
7,318件の閲覧回数
CompilerGuru
NXP Employee
NXP Employee
Yes, the compiler places global variables into .common (a special ELF section with a predefined ELF section index SHN_COMMON, but that should not matter).

E.g.:

int global_i;
7,318件の閲覧回数
ThomasH
Contributor II
And what is the .bss section?? For me it seems that the linker mixes .common and .bss section? Which types of variables will be linked there?
 
Thanks!
0 件の賞賛
返信
7,319件の閲覧回数
CrasyCat
Specialist III

Hello

Here are the predefined section used by the compiler is using:

.text : Contains the code.
.data : Contains the initialized global variables.
e.g. int a = 1, b= 2;
.stack: Contains the stack.
.bss : Contains the static un-initialized global variables.
e.g. static int c, d ;
.common: Contains the un-initialized global variables (not static).
e.g. int e, f;
.rodata : Contains the constant variables .
e.g. const int c1=2, c2=4 ;
.rodata1: Contains all the string constants.
e.g. #define mystr = “Hello world”

I hope this helps.

CrasyCat

0 件の賞賛
返信
7,317件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello CrasyCat and Pascal,

On CW10.6, S12Z chips , it seems no matter how i define the variable , it can not put in to the .bss segment .

For example

  int i = 0;

static int j ;

Why ?  And how can i put the variable to .bss segment ?

Thank !

Alice

0 件の賞賛
返信
7,318件の閲覧回数
DaveTonyCook
Contributor IV

Hi,

Just an addition to the above.  I'm working with CW 6.4 and it ignores the LCF *(COMMON) output section and sticks all uninitialised global data in the .bss section. !!??!!

I have the following:

1. static int x;          > .bss

2. static int y = 1;    > .data

3. static int y = 0;    > .bss   Couldn't this be quite dangerous as it relies on the start-up code zeroing the .bss. Uninitialised data should always be initialised before use.

4. int a                    > .bss  This should be emitted to .common or in this case *(COMMON) if provide the LCF however if I look at a disassembled c module the compiler does provide the required named section. This can be seen                                               by looking at the section index field (Shndx) in the symbol table.         

5. int a =1;              > .data

Also the linker documentation is very poor. Try searching the help file for COMMON, SCOMMON or .common ;0)

Snippet from my LCF

.uninitialized_data :

  {

  __START_BSS = .;

  *(.bss)

  . = ALIGN(0x8);

  # This should be for common GLOBAL variables declared in compiled code outside of any function

  # without the extern or static qualifier and which are not initialized. line has no effect!

  # All global uininitialised data declared as static,extern or with no type class specifier

  # are emmited to .bss TOGETHER WITH DATA INITIALISED TO 0

  *(COMMON)

  __END_BSS = .;

  . = ALIGN(0x8);

  } >> DATA

Any comments?

DaveCook

0 件の賞賛
返信
7,318件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Hi Dave,

the original post was for HC12 V4.5 architecture.

the linker parameter file is not the same for the HC12 architecture and Coldfire.

to check the issue I recommend you to create a new post for this question.

Be aware the Coldfire V6.4 is an old version.

the last version based on Classic IDE is the V7.2.

the last development for Coldfire is CW for MCU V10.4 based on Eclipse.

I could investigate the problem/question.

In this case can you please create a new post for this question.

regards

Pascal

0 件の賞賛
返信
7,318件の閲覧回数
DaveTonyCook
Contributor IV

Hi Pascal,

As far as I'm aware the .common section is part of the ELF standard and is independent of processor architecture. There are many people that use and do not properly understand boiler plate LCF supplied with the tool chain and there is no description in the linker documentation regarding this.  Also there are many people that use older versions of the CW IDE.  I would have thought from the title and content of this post that the general nature of the issue would be relevant on this thread.

Best regards

0 件の賞賛
返信
7,318件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Hi Dave,

I think I've understand the problem/question.

I need to work on it.

according to Catherine feedback the

      .common: Contains the un-initialized global variables (not static).

so in case of int a_1; the map file should use the SCOMMON or COMMON and not the .bss.

Regards

Pascal

0 件の賞賛
返信
7,318件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Hi Dave,

I've checked with compiler team and my understanding was correct.

      Both SCOMMON and COMMON are used for sections related to .common

Regards

Pascal

0 件の賞賛
返信