Unhandled Exception

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unhandled Exception

2,461 Views
Randhawa
Contributor I

Hi all,

 

I installed Code warrior S12 on my laptop .I created a project and when I clicked on one of the file created by IDE .It comes up with the window says

 

CodeWarrior encountered an unhandled exception 0xc0000005 at address 0x76148876

(The memory at address 0x02ffffe3 could not be written)

 

Location: USERS32.dll:0x76148876

 

Choose 'Abort'to end the program ,'Retry' to debug or 'Ignore' to continue

 

When I click on Ignore then comes up with another error message

 

Code warrior encountered an unhandled C++ exception

 

Choose 'OK' to terminate the program

 

OS: WIndow7 professional

Memory: 4GB

 

if somebody have any solution to fix this problem that would be appriate for me.

 

Thanks

Labels (1)
Tags (1)
0 Kudos
Reply
2 Replies

1,810 Views
CrasyCat
Specialist III

Hello

 

Did you check this post:

https://community.freescale.com/message/52944#52944

 

CrasyCat

0 Kudos
Reply

1,810 Views
Randhawa
Contributor I

I tried it .But this doesn't work !!!

 

0 Kudos
Reply