Unexpected status of script:...Kinetis.rgi in CW 10.6 for MKL24Z64VLH4

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unexpected status of script:...Kinetis.rgi in CW 10.6 for MKL24Z64VLH4

1,177 Views
bobnayar
Contributor II

I had a project using the MKL24Z64VLH4 processor that was compiling and building fine.

I am using a licensed copy of CW 10.6

 

All of a sudden, after an update, I am getting this error:

Unexpected status of script: Drivers\Kinetis\Kinetis.rgi, please contact Freescale Support.

 

I can't generate any of the PE code for the processor and so I am dead in the water.

Please let me know how I can solve this,.

Thanks.

 

Bob N

Labels (1)
0 Kudos
Reply
2 Replies

1,010 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi

I never had same problem as yours,

I wonder if some of the CW system file was corrupt? can you please reinstall CW and update, then test a new created project in a new workspace? how does it work?
Have a great day,
Zhang Jun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,010 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Bob,

Please tell me which patch do you update ? And also tell me how can i reproduce the problem step by step.

And you can try create a new workspace ,  then create a new project ,then check whether it can work well .

BR

Alice

0 Kudos
Reply