Undefined error from Compiler, but not from IDE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Undefined error from Compiler, but not from IDE

ソリューションへジャンプ
4,305件の閲覧回数
marcbunyard
Contributor IV

I'm getting a compiler error where the compiler says that it has an undefined variable, yet the IDE is able to find it through "Open Declaration".  All of the include paths seem to be intact, but the compiler errors on the same variable.

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
4,042件の閲覧回数
BlackNight
NXP Employee
NXP Employee

The error only disappeared because the preprocess 'compile' was sucessful. About the output console: I have it the preprocessor listing in a new window/source file. I'm using gcc.

元の投稿で解決策を見る

0 件の賞賛
返信
7 返答(返信)
4,042件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Could you post the exact error message? Which compiler/target?

I recommend that you generate a preprocesing listing: I guess there is something wrong with your includes, or with the defines.

The fact that the IDE does not find the declaration too really could mean that your includes are not correct.

I hope this helps.

0 件の賞賛
返信
4,042件の閲覧回数
marcbunyard
Contributor IV

The IDE DOES find the declaration.  That's what's confusing.  Here's a screen capture of the error after the compile:

UndefinedError.png

I'm  trying to figure out how to get the pre-processor listing (still new to Code Warrior).

Thank you.

0 件の賞賛
返信
4,042件の閲覧回数
BlackNight
NXP Employee
NXP Employee

ah, sorry, I thougth the IDE was not able to find it.

Preprocessor listing: you should be able to right click on the source file, and the context menu should offer you that.

Maybe the order of includes is the problem?

0 件の賞賛
返信
4,042件の閲覧回数
marcbunyard
Contributor IV

Interesting.  I right clicked on preprocess, it ran the preprocessor, and the errors were removed!  So I ran the build, and they're back!?  To add another level to the confusion, this project compiles, but won't link, under RAM, but not FLASH (hvac_wifi).  I haven't changed the include file order from what it was when shipped as a Freescale example.  The hvac_wifi example appears to be written for the K60M100, and I am building it for the K60M120.  The startup code for the M100 would not work for the M120.  It hung on the PLL setup.

When I ran the preprocessor, the listing was output on the console.  After doing the build, it stopped outputing it on the console. ???

0 件の賞賛
返信
4,043件の閲覧回数
BlackNight
NXP Employee
NXP Employee

The error only disappeared because the preprocess 'compile' was sucessful. About the output console: I have it the preprocessor listing in a new window/source file. I'm using gcc.

0 件の賞賛
返信
4,042件の閲覧回数
marcbunyard
Contributor IV

The preprocessor was a good suggestion.  I clicked on disassembly below it, and got an error I hadn't seen before.  It was a missing include path that kept me from including "verif_user_config.h".  It compiles ... now ... does it run?!?!?

Thank you.

4,042件の閲覧回数
marcbunyard
Contributor IV

The preprocessor was a good suggestion.  I clicked on disassembly below it, and got an error I hadn't seen before.  It was a missing include path that kept me from including "verif_enabled_config.h".  It compiles ... now ... does it run?!?!?

Thank you.

0 件の賞賛
返信