USB driver issue????

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

USB driver issue????

跳至解决方案
3,211 次查看
jigsaw
Contributor I
I installed CodeWarrior Development Studio for S12(X) V5.0 on my pc every time i plugin my HSC12E128 board it asks for a driver and than says driver not installed where do i get  the driver from.. thx
标签 (1)
标记 (1)
0 项奖励
回复
1 解答
2,433 次查看
J2MEJediMaster
Specialist I

OK, as you have figured out, the board has a S08 part and therefore CodeWarrior for HCS12(X) is not going to work with the board.

 

Have you followed the step-by-step instructions in the DEMO9S08LL16 Quick Start document? You have to install a service pack, and then the DemoLL16_Toolkit_setup executable to install the P&E utilities. All of this software should be on the DVD that came with the board.

 

When you plug the board into the USB cable for the first time, you should get a prompt to install new drivers. You pick the Recommended Option, which then installs the drivers that came with the CodeWarrior installation.

 

---Tom

在原帖中查看解决方案

0 项奖励
回复
3 回复数
2,433 次查看
J2MEJediMaster
Specialist I

What version of Windows are you using? If, during the installation, did you see any notices about drivers being installed, and if you did, did you allow them or block them? If you blocked them, a driver might not have been installed.

 

---Tom

0 项奖励
回复
2,433 次查看
jigsaw
Contributor I

Well at first i installed it on windows 7 than i knew it was not compatible with it.. so i installed it on XP but again the same problem.. was not detectng the driver...

 

P.S. Do you know what version of codewarrior is used with DEMO9S08LL16 board.. my uni gave me codewarrior v6.x but it dosent show me the board name when i start the software..

 

Thx

Jigsaw. 

0 项奖励
回复
2,434 次查看
J2MEJediMaster
Specialist I

OK, as you have figured out, the board has a S08 part and therefore CodeWarrior for HCS12(X) is not going to work with the board.

 

Have you followed the step-by-step instructions in the DEMO9S08LL16 Quick Start document? You have to install a service pack, and then the DemoLL16_Toolkit_setup executable to install the P&E utilities. All of this software should be on the DVD that came with the board.

 

When you plug the board into the USB cable for the first time, you should get a prompt to install new drivers. You pick the Recommended Option, which then installs the drivers that came with the CodeWarrior installation.

 

---Tom

0 项奖励
回复