The CodeWarrior IDE version 5.9.0 (CodeWarrior Professional version 8.8)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The CodeWarrior IDE version 5.9.0 (CodeWarrior Professional version 8.8)

3,864 Views
maryo
Contributor I

Hi,

I have recently installed CW professional Version 8.8.

After the installation, I used the CW updater to install the service pack " CodeWarrior
Power Architecture 8.8 Service Pack 2” for MPC8306, MPC8308 and MPC8309.
" (since I intend to used CW on the MPC8309kit board).

When I start the flash programmer (tools/flash programmer/Target Configuration), the target processor 8309 is not available in the 83xx family.

Question:

What should I do more in order to add the target processor 8309 to the 83xx family?

Thanks

CW mpc8309 not present.JPG  

Tags (1)
0 Kudos
Reply
2 Replies

3,631 Views
maryo
Contributor I

Thank you for your reply Pavel.

But as I am saying in the description, I have done what you suggested but it is still not helping.

So I guess there is something else I ned to do.

0 Kudos
Reply

3,630 Views
Pavel
NXP Employee
NXP Employee

Load and install the CW PA v8.8 for 830606S-8308-8309 Windows-hosted Service Pack.

See attached snapshot.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply