Storing data to flash in k20d72m

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Storing data to flash in k20d72m

1,269 Views
josephxavier
Contributor III

please share me a code to store data to flash (my need is to retain data even after power off ) , I am using K20D72M development kit.

what is the starting address for user data to be stored in flash?

Labels (1)
0 Kudos
Reply
1 Reply

1,188 Views
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello josephxavier:

Thank you for posting this question.

If you intend to use the FlexNVM functionality to store data, then in the next discussion you can find an example project attached to the response of colleague Carlos Casillas:

Re: FlexNVM Read/Write?

There is an application note to understand the whole FlexMemory system (AN4282) and the address space to be used:

http://cache.nxp.com/files/32bit/doc/app_note/AN4282.pdf

I hope this information is helpful.


Best Regards!
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply