Sharing CWS4.5 (for HCS12X) with 2 dongles for 3 users

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Sharing CWS4.5 (for HCS12X) with 2 dongles for 3 users

跳至解决方案
1,979 次查看
MickLauffer
Contributor I
Hi

We plan to upgrade our 2 existing CodeWarrior licenses (v3.1 for HC12S) to the newest version (4.5 for HCS12S).
So far we worked with licenses tied to the hardware-ID but now we plan to buy USB dongles in order that more than 2 people may share those two licenses. Will it work like that, e.g. that those 2 dongles are used on 3 different PCs (in different combinations) or is it like that one PC works only with a dedicated dongle (which may be shared for different PCs)? Or in different words: does it matter which dongle is attached to the PC or is it possible to have a "pool" of dongles for different PCs?

TIA,
Mick

Message Edited by Mick Lauffer on 2007-04-1611:35 AM

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,274 次查看
Alban
Senior Contributor II
Hello Tom & Mick,

licensing@metrowerks.com seems not to be transferred to @freescale.com (not in the list)

Emails to license@freescale.com are received for sure.

The other option is always to create a Service Request :smileyhappy:

Cheers,
Alban.


在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,274 次查看
J2MEJediMaster
Specialist I
I think you can share the dongles around, but check this forum thread. E-mail licensing@freescale.com for a definitive answer.

---Tom
1,275 次查看
Alban
Senior Contributor II
Hello Tom & Mick,

licensing@metrowerks.com seems not to be transferred to @freescale.com (not in the list)

Emails to license@freescale.com are received for sure.

The other option is always to create a Service Request :smileyhappy:

Cheers,
Alban.


0 项奖励
回复