S29JL032J70TFI32

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S29JL032J70TFI32

2,234 Views
lixinhua
Contributor I

Dear Sir ;

 

I can not find "S29JL032J70TFI32" in Flash Driver of CW_ColdFire_7.2 , Could you help me to supprot it ?

 

Best Regards ;

 

TIM

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

2,062 Views
TICS_Fiona
NXP Employee
NXP Employee

Hello xinhua

The S29JL032J70TFI32 is not in the list of Flash_Programmer devices that supported:

..\Freescale\CodeWarrior for ColdFire V7.2\bin\Plugins\Support\Flash_Programmer\ColdFire

Please create it following 6.3 in AN3389:

http://cache.nxp.com/files/soft_dev_tools/doc/app_note/AN3389.pdf

I would recommend updating to latest CodeWarrior version v10.6.4, it supports some flash device from Spansion. It can be downloaded from:

CodeWarrior for Microcontrollers-Eclipse IDE|NXP

Its update v10.6.5 and v10.6.6 are also available at the same link.

Best Regards

Fiona Kuang

TIC - Technical Information Center

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Mark Correct button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply