S Record Meaning

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,439件の閲覧回数
kackle123
Contributor IV

I see that in an S record that an "S9" record/line is supposed to describe a starting execution address.  But when I decode that line, the address is nowhere near that actual starting address of the firmware.  It seems simple to understand; am I missing something?

0 件の賞賛
返信
1 解決策
2,356件の閲覧回数
ErichStyger
Specialist I

Hi,

What tool did you use to generate the S19 file (I assume the GNU objcopy)?

The address can be omitted (or set to zero) depending on the tool which generates it. But the GNU objcopy should set it to the start address which is usually the reset vector:

pastedImage_1.png

I hope this helps,

Erich

PS: Decoding S19 Files | MCU on Eclipse 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,356件の閲覧回数
kackle123
Contributor IV

You can see my incorrect thinking in my post: "...starting address of the firmware."  My S record file starts its firmware bytes at 0x8000 (vector table, constants, etc.), but the actual beginning of the executable part of the program (the reset vector) IS correctly defined by the S9 record/line.  Now it makes sense.  Thank you for helping me think through it, Erich.

0 件の賞賛
返信
2,357件の閲覧回数
ErichStyger
Specialist I

Hi,

What tool did you use to generate the S19 file (I assume the GNU objcopy)?

The address can be omitted (or set to zero) depending on the tool which generates it. But the GNU objcopy should set it to the start address which is usually the reset vector:

pastedImage_1.png

I hope this helps,

Erich

PS: Decoding S19 Files | MCU on Eclipse 

0 件の賞賛
返信