Read image from device

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Read image from device

ソリューションへジャンプ
6,030件の閲覧回数
ChrisTango
Contributor IV

Hello everybody,

 

I'm using Codewarrior 10.5, a P&E micro USB Multilink Interface and having a S08 microcontroller on my board.

 

So, basically I'm only searching for a way to read out the image, but I can't find menu for this kind of work.

Does anybody know how I can do this? I'm able to Flash and debug so the Connection should work fine.

 

Thanks and best regards,

Chris

ラベル(1)
1 解決策
5,014件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Chris:

You can do this as explained in the next tutorial:

Dump my Device Memory | MCU on Eclipse


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

5 返答(返信)
5,014件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Chris:

You can do this as explained in the next tutorial:

Dump my Device Memory | MCU on Eclipse


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

5,014件の閲覧回数
ChrisTango
Contributor IV

Hello Jorge,

Thanks, this will work out for me! I just got a dump from my chip and it seems to be correct. :-)

Best regards,

Chris


0 件の賞賛
返信
5,014件の閲覧回数
takaoyamada
Contributor IV

Greetings,

Within Codewarrior you will only be able to look at the data in flash and RAM while debugging the hardware. But if you want to read the flash and dump it into a file, then I would suggest getting the PROGHCS08 software from P&E and use the command "upload module" to dump the file as an S19 file.

P&E Microcomputer Systems - PROGHCS08 - 68HCS08 Flash/EEPROM Programmer Software - HCS08, Flash/EEPR...

Note, if the chip is secured and have not setup a backdoor key, then there is no way of reading the flash. You would need to unsecure the chip, which involves erasing all of flash and EEPROM.

Takao Yamada

P&E Microcomputer Systems

5,014件の閲覧回数
hiphopbalance
Contributor I

Is there a free version of the proghcs08 ? Cause your link is to a very expensive software.

0 件の賞賛
返信
5,014件の閲覧回数
ChrisTango
Contributor IV

Hi Takao,

Thank you for this hint! When I need more advanced Features or I've to do it more often then I will use the PROGHCS08 tool.

I've an unsecure sample, so I've access to it.

Best regards,

Chris


0 件の賞賛
返信