Question regarding MC9S12XHZ256 microcontroller.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Question regarding MC9S12XHZ256 microcontroller.

1,420 次查看
walterbarrer
Contributor I

I have an instrument cluster that uses the MC9S12XHZ256 MCU. The cluster gets a "Failed Self test" message on it's LCD Odometer display when the ignition voltage is applied.I can verify the MCU is the failure by swapping in a known good one. In the "bad" MCU, all of the odometer information has been erased. Other than that , the cluster performs normally. Because of this, I'm thinking that it's an EEPROM issue as opposed to a Flash memory issue.If this is correct, can the EEPROM in the failed MCU be reprogrammed? Does NXP have a programmer that supports this device? Thanks.

Walt Barrer

[email protected]

0 项奖励
回复
1 回复

1,253 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi

Can on-chip BDM interface function well? if yes, I recommend "PROG12Z 68HC(S)12(X) Flash/EEPROM Programmer Software"

PEmicro - P&E Microcomputer Systems: Over 30 years as an Industry leader in Embedded Systems Develop... 

I would suggest you consult P&E for more information about it.


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复