Question for CAN acceptance filter(extended)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Question for CAN acceptance filter(extended)

1,190 次查看
trunie
Contributor I

Hi. I am Kim from South Korea.

Now I have to use the CAN acceptance filter for extended id.(not standard id.)

(Last year I got an answer for standard filter from here and I complete it)

The id. That I should receive is 0x18ff56e7 and I set the code warrior as below.

52743_52743.jpg제목 없음.jpg

 

Thank you.

Best regards.

Kim.

标签 (1)
0 项奖励
回复
1 回复

1,028 次查看
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Kim,

Could you tell us the MCU and CodeWarrior version being used?

Regarding the acceptance filter, please remember that the acceptance filters are applied to the full 29 bits of the extended identifier and to the following bits of the CAN 2.0B frame: Remote transmission request (RTR), Identifier extension (IDE) and Substitute remote request (SRR).

pastedImage_0.png

So you should consider these bits in your acceptance code.

Best Regards,

Carlos Mendoza

Technical Support Engineer

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复