Programming HCS08 on Raspberry Pi

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Programming HCS08 on Raspberry Pi

2,910件の閲覧回数
edasanli
Contributor I

I need to programming MC9S08PA4 on Raspberry Pi. I tried to install Code Warrior on RPi, but RPi is based on ARM so it could not install. I don't need to developing, I have a s19 file, just need to programming my microprocessor.

Is there someone have a solution about that? 

Have a nice day. 

-Eda 

#mc9s08pa4‌raspberry pi‌

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

2,854件の閲覧回数
vicentegomez
NXP TechSupport
NXP TechSupport

Hi

In order to program the S08 you will need an OSBDM, those are available on several evaluation boards or in programmers like the Universal multilink from P&E.

or you can create your own OSBDM, please check 

PEmicro | Experts in Embedded tools for Flash Programming and Development 

I hope this will help you

Regards

Vicente 

0 件の賞賛
返信

2,854件の閲覧回数
edasanli
Contributor I

I have S08PT60-EVK and PE Micro Multilink. But I need an application for programming, which can be installed on Raspberry Pi.

0 件の賞賛
返信