Program running out

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Program running out

2,334 Views
gm2010ustc
Contributor I

XEP100 MCU,When the program runs into the update function,run to PFlash_EraseSectorBySector(0x7C0000UL, 0x7FDFDFUL);

when  this program is run over,it  jump directly to the ZeroMem function,then the Program running out.  I don't know why this happen.

Original Attachment has been moved to: bootloader_debug_20151030.rar

Labels (1)
0 Kudos
Reply
3 Replies

2,156 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

this thread was posted two years ago.

Please create a new thread for your specific question.

I would suggest you attach the error screenshot and demo project of the problem.

Jennie Zhang

0 Kudos
Reply

2,156 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

hi,

I have answered you in SR1-4142120521,

please refer the demo code to make your own project.

thanks!


Have a great day,
Zhang Jun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,156 Views
tafengchung
Contributor II

I have the same question,

why? and how to fixed this issue?

0 Kudos
Reply