Processor Expert for MM9Z1_638?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Processor Expert for MM9Z1_638?

1,260 Views
yin
Contributor I

I am using MM9Z1_638 with CodeWarrior free version. I can not find a way to use processor expert with this chip and I wonder whether it is supported. Thanks.

Labels (1)
0 Kudos
Reply
1 Reply

1,166 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi

So far processor expert doesn't support MM9Z1_638. and there is no plan to develop processor expert for MM9Z1_638 in near feature.

If I got any news on this regard, I will also keep you update.


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply