Processor Expert for MM9Z1_638?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Processor Expert for MM9Z1_638?

1,236件の閲覧回数
yin
Contributor I

I am using MM9Z1_638 with CodeWarrior free version. I can not find a way to use processor expert with this chip and I wonder whether it is supported. Thanks.

ラベル(1)
0 件の賞賛
返信
1 返信

1,142件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi

So far processor expert doesn't support MM9Z1_638. and there is no plan to develop processor expert for MM9Z1_638 in near feature.

If I got any news on this regard, I will also keep you update.


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信