Problems of the code generated by lin stack configuration tool(NCFTool)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problems of the code generated by lin stack configuration tool(NCFTool)

2,388件の閲覧回数
jeffcharles
Contributor III

Hi,

I am using the NCF tool to generate three configuration files. I found something wrong with the interface function in lin_cfg.h:

The signal size of 'S2M_Sig3' is 3 and the offset is 6, so bit 6 and bit 7 of byte 1 and bit 0 of byte 2 in the signal array 'lin_pFrameBuf' is occupied by it.pic2.JPG

But the following macro only access the byte 1 about 'S2M_Sig3', why?

pic3.jpg

Please give me support. Thank you!

Jeff

0 件の賞賛
返信
2 返答(返信)

2,371件の閲覧回数
dianabatrlova
NXP TechSupport
NXP TechSupport

Hi Jeff,

 

Could you, please, specify which MCU you use?

Thank you.

Best regards,

Diana

0 件の賞賛
返信

2,357件の閲覧回数
jeffcharles
Contributor III

Hi Diana,

I am using the MC9S12ZVL32

 

Best Regards,

Jeff

0 件の賞賛
返信