Problems loading legacy project from Metrowerks Codewarrior into Codewarrior for HCS12(X) v5.1

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problems loading legacy project from Metrowerks Codewarrior into Codewarrior for HCS12(X) v5.1

ソリューションへジャンプ
29,414件の閲覧回数
richardscott
Contributor I

Hello, I have a legacy project from Metrowerks Codewarrior (v5.5.1272, dated 2003) which I have loaded into Codewarrior for HCS12(X) v5.1 Evaluation Version (I can't use v5.2 as the CPU - MC9S12D64BCPV isn't supported).

 

The project will not compile, as there are errors in the CPU configuration (see attached screenshot). The CPU configuration has no errors in the old Metrowerks IDE. 

 

I'd like to know if the evaluation limitations are the root cause of this problem, or if there is something more complicated going on, or if I am doing something stupid. I don't have any hardware attached yet, if that makes any difference, I just want to be able to run 'make'.

 

Thanks.

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 解決策
29,318件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Richard,

in your screenshot, the memory configuration is  not correct. please refer below to correct it

pastedImage_1.png

if this can not help, please upload your project thus we can check it directly.


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
29,319件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Richard,

in your screenshot, the memory configuration is  not correct. please refer below to correct it

pastedImage_1.png

if this can not help, please upload your project thus we can check it directly.


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
29,318件の閲覧回数
richardscott
Contributor I

Thank you.

This corrected the configuration error (I'm guessing due to stricter error checking in the newer version) but the code still won't compile due to other errors. I'll open a private support ticket so I can send the code.

Richard.

0 件の賞賛
返信
29,318件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

fine. Thanks.

your private ticket was just answered.

Jennie

0 件の賞賛
返信