Problem compiling eGUI library

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem compiling eGUI library

3,034 Views
Glogov_Kolac
Contributor II

I have an problem when I include D4D eGUI library into my project. When I try to build it, this process never ends. On some % building stops and have no progress (I wait it for one hour). I use D4D libraryy source files and code examples for Official Demo (for Kinetis K60 Tower). Is there some special procedure to include D4D in custom project and to compile it with success ?

Labels (1)
0 Kudos
Reply
3 Replies

2,782 Views
infoterm
Contributor I

I have same problem when I want to integrate eGUI in my project, like it is doed in Official Example. Here is my project! Compiling never stops, it stuck at d4d_base compiling infinitevly !!!

0 Kudos
Reply

2,782 Views
infoterm
Contributor I

I try to integrate D4D into my project, instead of using eGUI Official Demo. Same situation, compling infinitevly. I request support from Freescale but they don't answer. I try D4D on 4 different computers and 3 different projects and it only works with official demo. !!!

0 Kudos
Reply

2,783 Views
J2MEJediMaster
Specialist I

See if this https://community.freescale.com/message/94424#94424 has the solution for you.

 

---Tom