Post-linker in CW classic

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Post-linker in CW classic

2,001 Views
bengtandersson
Contributor III

I trying to get some information on how to create a Post-linker. I have understand that it is some kind of .bat file but I cant find any information about commands and syntax to be used. The help in CW just tells me to "see the appropriate Targeting manual" and I don't understand where to find it.

 

I'm using CodeWarrior Development Studio for S12(X) Version 5.1 , build 10221

 

/Bengt Andersson

Labels (1)
0 Kudos
Reply
3 Replies

1,853 Views
BlackNight
NXP Employee
NXP Employee
0 Kudos
Reply

1,853 Views
bengtandersson
Contributor III

Hi!

Already seen it and it is a great help if you have a .bat file and just want to run automatically when you build the project. What I look for are instructions on how to build a bat file from scratch, utilizing all available commands. Is it just common Windows command line commands or are there special commands only used in CW?

//Bengt

0 Kudos
Reply

1,853 Views
BlackNight
NXP Employee
NXP Employee

Hi Bengt,

it is just common Windows command line commands.

Erich

0 Kudos
Reply