OSBDM and ICG trim

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

OSBDM and ICG trim

3,201 Views
peg
Senior Contributor IV
Hello,
When using the Open Source BDM, how are you meant to calculate and then programme the non volatile version of the ICG trim value?
 
BR Peg
 
Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

1,172 Views
peg
Senior Contributor IV

OK,

I figured out I can write a small cmd file to write the value to FLASH using the FCMD register. Now to calculate the value....

Well I can calculate the value required too with technique from AN2496 but this hardly compares to the ease of use with P&E's BDM.

How do they do it? or is there already a way within Hiwave?

BR Peg

 

Message Edited by peg on 04-16-200610:51 PM

0 Kudos
Reply