Librarian not accepting -Cmd

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Librarian not accepting -Cmd

2,462 Views
omermajeed
Contributor I

Hello,

 

I am using makefiles to build the project, and there I am trying to make a library out of some object files.

Compiler is doing fine, it is making all the object files correctly. But when I try making library using -cmd command librarian fails to do so.

 

AR_COMMAND = C:\Freescale\CWMCUV~1.6\MCU\S12lisa_Tools\Build_Tools\libmaker  -WmsgNu=abc -Cmd{$(OBJS) = $(LIBNAME)}

 

AR_COMMAND is used to make library with name = LIBNAME, OBJS has all the object files make by compiler.

 

Does anybody has any idea what's wrong with the AR_COMMAND?

 

Best Regards,

Omer

Labels (1)
0 Kudos
Reply
1 Reply

2,291 Views
trytohelp
NXP Employee
NXP Employee

Hi Omer,

By default when you create an example with the wizard you can select between Application or library.

I've created a project for library and build it.

Extract of console:

+++++++++++++++++++++++

**** Clean-only build of configuration Debug for project test_lib_s12lisa ****

Build complete for project test_lib_s12lisa

**** Build of configuration Debug for project test_lib_s12lisa ****

"E:\\Freescale\\CW_MCU_v10.6\\gnu\\bin\\mingw32-make" -j8 all

'Building file: ../Lib/mylibrary.c'

'Executing target #1 ../Lib/mylibrary.c'

'Invoking: S12Z Compiler'

"E:/Freescale/CW_MCU_v10.6/MCU/S12lisa_Tools/Build_Tools/mwccs12lisa" -c @@"Lib/mylibrary.args" -o "Lib/mylibrary_c.obj" "../Lib/mylibrary.c" -MD -gccdep

'Finished building: ../Lib/mylibrary.c'

' '

'Building target: test_lib_s12lisa.lib'

'Executing target #2 test_lib_s12lisa.lib'

'Invoking: S12Z Libmaker'

"E:/Freescale/CW_MCU_v10.6/MCU/S12lisa_Tools/Build_Tools/libmaker" -NoPath  -cmd(  "./Lib/mylibrary_c.obj"    = "test_lib_s12lisa.lib")

- ./Lib/mylibrary_c.obj

- E:\Temp_bis\Community\355016\MCU_10.6\test_lib_s12lisa\Debug\test_lib_s12lisa.lib

Listing of 'test_lib_s12lisa.lib' is written to 'E:\Temp_bis\Community\355016\MCU_10.6\test_lib_s12lisa\Debug\test_lib_s12lisa.lst'

'Finished building target: test_lib_s12lisa.lib'

' '

+++++++++++++++++++++++

May be there is an issue with the path.

Have a great day,
Pascal
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply