Is there support for k61 on linux?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is there support for k61 on linux?

1,103件の閲覧回数
chucktilbury
Contributor I

My preferred development platform is Linux and I am working with the k61 processor. We are using CW version 10.6 under windows for this. I want to know if there is similar support for the processors that v10.6 supports for Linux.

0 件の賞賛
返信
1 返信

1,059件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

HI

we don't have a CW10.6 version that can support linux. for CW10, only CW10.2 have linux version but it's too old.

I suggest you use MCUXpresso instead which can support linux.

MCUXpresso IDE|NXP 


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信