In-line assembly in Codewarrior for 8 bit v6.2

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

In-line assembly in Codewarrior for 8 bit v6.2

跳至解决方案
4,276 次查看
RakeshParekh
Contributor I

Hi,

 

I am developing code using MC9S08QD2 and codewarrior v6.2

 

For certain critical operations, I want my generated code to be optimized in size and execution speed.

 

Are there ready to use intrinsic functions defined in codewarrior to use assembly instructions like ROR - rotate right through carry, SEC - set carry, CLC - clear carry etc?

 

As I do not find these intrinsic function, I tried to put down macro definition for these purpose.

 

However it does not compile.

For ex.
unsigned char VarC;
#defined RotateRight(x) {__asm ROR x;}

void main (void)
{
:
:
RotateRight(VarC);
:
}

I get compiler error messages C18700 and C18701.

How to resolve it?

Same error messages go away if I first transfer operand to accumulator and work on accumulator.

Why so?
 
Kindly advice asap.
 
Thanks and regards,
 
Rakesh

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
2,848 次查看
CompilerGuru
NXP Employee
NXP Employee

The ROR instruction does only support DIR (meaning 8 bit addresses) and not EXT (meaning 16 bit addresses). Therefore either allocate VarC in a __DIRECT_SEG area (and tell the compiler), load, rotate in a register, rotate the register and store it back to VarC or load the address of VarC into H:X and use "ROR ,X".

 

I'm guessing that placing the variable into a __DIRECT_SEG segment is the best way to go as this is an optimization task.

E.g.

#pragma push#pragma DATA_SEG __SHORT_SEG MY_NEAR_DATA_SEG  // must be mapped in the prmunsigned char VarC;#pragma pop

 

 

Check the ROR access details in the HCS08 reference manual and AN2093.pdf also contains samples using the direct page.

 

Daniel

在原帖中查看解决方案

0 项奖励
回复
4 回复数
2,849 次查看
CompilerGuru
NXP Employee
NXP Employee

The ROR instruction does only support DIR (meaning 8 bit addresses) and not EXT (meaning 16 bit addresses). Therefore either allocate VarC in a __DIRECT_SEG area (and tell the compiler), load, rotate in a register, rotate the register and store it back to VarC or load the address of VarC into H:X and use "ROR ,X".

 

I'm guessing that placing the variable into a __DIRECT_SEG segment is the best way to go as this is an optimization task.

E.g.

#pragma push#pragma DATA_SEG __SHORT_SEG MY_NEAR_DATA_SEG  // must be mapped in the prmunsigned char VarC;#pragma pop

 

 

Check the ROR access details in the HCS08 reference manual and AN2093.pdf also contains samples using the direct page.

 

Daniel

0 项奖励
回复
2,848 次查看
RakeshParekh
Contributor I

Pls. ignore Solved Tag.

 

It was by mistake.

 

The issue is not solved.

 

Thanks and regards,

 

Rakesh

0 项奖励
回复
2,848 次查看
RakeshParekh
Contributor I

Hi,

 

VarC is declared in direct page area. In map file, its location is 0x87.

 

But still error comes.

 

Is #pragma push and #pragma pop necessary in definition?

 

what they do?

 

Kindly advice.

 

Thanks and regards,

 

Rakesh

0 项奖励
回复
2,847 次查看
CompilerGuru
NXP Employee
NXP Employee

> VarC is declared in direct page area. In map file, its location is 0x87.

 

Is is declared in a section with a __SHORT_SEG qualifier? The compiler does not read map files Smiley Wink.

It's the other way round, if the variable is placed in a  __SHORT_SEG section and that section is placed in the prm file into the first 256 bytes, then the map file will show an address < 256.

 

 

Here a simplistic snippet which works for me:

 

 

 

#pragma DATA_SEG __SHORT_SEG MY_ZEROPAGEunsigned char VarC;#define RotateRight(x) {__asm ROR x;}void main (void){  RotateRight(VarC);}

 

Also note the manuals in the help and help\pdf folders.

 

Daniel

 

 

0 项奖励
回复