Import K60F120M SC to CodeWarrior 10.3

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Import K60F120M SC to CodeWarrior 10.3

1,825件の閲覧回数
bodie
Contributor I

Hello,

I have Twr-K60F120M and I want to load into this board demo program. I found and download KINETIS_120MHZ_SC, but I don't know how right import it into VW 10.3 and load into MCU?

Thanks for reply

 

Tomáš

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,545件の閲覧回数
michalmrosko
Contributor I

Hello Tomáš,

The way, how to do it, is described in cw_readme.txt file, which is placed in directory KINETIS_120MHZ_SC\build\cw.

0 件の賞賛
返信

1,545件の閲覧回数
bodie
Contributor I

Thanks for answer, but I made a mistake in my question. There is no problem with importing KINETIS_120MHZ_SC. I want to load into mcu the demo program, which should be in it at the beginning. I download them on freescale web (TWR-K60F120M_QSD.zip) and now I have the code, but dont know how to import it to CW, because it isn't VW project, only single files or IAR project. Anybody know?

0 件の賞賛
返信