Import 8.3 codewarrior project into codewarrior 10.4

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Import 8.3 codewarrior project into codewarrior 10.4

Jump to solution
3,069 Views
lynnschneider
Contributor I


Having problem importing.

Labels (1)
0 Kudos
Reply
1 Solution
2,638 Views
TICS_Fiona
NXP Employee
NXP Employee

CodeWarrior v10.5 includes CodeWarrior Classic Project Importer for CW DSC v8.3 projects, but CW v10.4 does not.

CodeWarrior v10.5 can be downloaded from:

http://tinyurl.com/6jo5tge

If you would use CW10.4, the solution is user needs to create a new bareboard project in CW10.4 and then add/copy all your source files to the new project.  For a project with PE, user also have to add the PE component manually.

Below is an application not for how to do this:

http://cache.freescale.com/files/soft_dev_tools/doc/app_note/AN4727.pdf

View solution in original post

0 Kudos
Reply
5 Replies
2,638 Views
lancefisher
Contributor III

I spent two hours downloading and installing version 10.5 but I can't find anything in the help system that explains how to import a project from CW 8.3.  Also in CW 8.3 it appears that the Export Project function doesn't generate anything except an xml file with some project settings.  I think I'd need more than that to import into CS 10.5.  What is the procedure for exporting from 8.3 and importing into 10.5 or where do I find this information?

0 Kudos
Reply
2,638 Views
Ben
Senior Contributor I

Lance, I import old project to 10.5 directly from 10.5 menu file>import

In the selection window select the CodeWarrior folder and the "CodeWarrior Classic Project".

It worked for me. No special export preparations in 8.3 needed.

0 Kudos
Reply
2,639 Views
TICS_Fiona
NXP Employee
NXP Employee

CodeWarrior v10.5 includes CodeWarrior Classic Project Importer for CW DSC v8.3 projects, but CW v10.4 does not.

CodeWarrior v10.5 can be downloaded from:

http://tinyurl.com/6jo5tge

If you would use CW10.4, the solution is user needs to create a new bareboard project in CW10.4 and then add/copy all your source files to the new project.  For a project with PE, user also have to add the PE component manually.

Below is an application not for how to do this:

http://cache.freescale.com/files/soft_dev_tools/doc/app_note/AN4727.pdf

0 Kudos
Reply
2,638 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

please refer an4727  for how to port classic CW to eclipse:

http://cache.freescale.com/files/soft_dev_tools/doc/app_note/AN4727.pdf

2,638 Views
tonywu
Contributor I

What about the PE settings? Shouldn't Freescale provide a easier tool to convert?

0 Kudos
Reply