How to reference an absolute address defined in PRM file by a symbol for S12 MCU?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to reference an absolute address defined in PRM file by a symbol for S12 MCU?

3,543件の閲覧回数
007
Contributor II

Hello Freescale,

 

I have a question as title. Here is my case, in S12 PRM file, a flash section is allocated at 0xC000 area, and in code, I want to do a flash checksum checking using the address.  I think the compiler can use a symbol in C code to refer or extern to the absolute address in PRM file, in stead of re-define this address in C code. I see TI MCU compiler has this usage,  an address symbol can be defined in its memory control file, and it can be used in C.

 

In following example, how to reference ROM_C000_Start, ROM_C000_End and Rom_Cs_Word?

 

project.prm:

 

SEGMENTS

... ...

ROM_CS          = READ_ONLY     0xC000 TO   0xC001;

ROM_C000       = READ_ONLY     0xC002 TO   0xEFFF;

... ...

END

 

PLACEMENT

... ...

APP_ROM     INTO      ROM_C000

... ...

END

 

 

C code:

void Startup (void)

{

     U16 cs;

     cs = Checksum_CheckAreaWordAdd (ROM_C000_Start, ROM_C000_End);

     if (cs != *(U16 *) Rom_Cs_Word)

     {    

          for(;;);

     }

     ... ...

}

 

Regards,

dp

ラベル(1)
タグ(4)
0 件の賞賛
返信
3 返答(返信)

3,048件の閲覧回数
kef2
Senior Contributor V

There are linker predefined symbols __SEG_STARTxxxx and __SEG_ENDxxxx. But these don't work with entries from  SEGMENTS. They work with entries from PLACEMENT

extern char __SEG_START_APP_ROM[]; // have to be extern array of charss

extern char __SEG_END_APP_ROM[];  // -"-

   void *start, *end;

   start = &__SEG_START_APP_ROM;  // yes, address of "address"

   end = &__SEG_END_APP_ROM;  // -"-

start and end will be NULL, if there's no APP_ROM PLACEMENT, or if there's nothing placed to APP_ROM.

0 件の賞賛
返信

3,048件の閲覧回数
007
Contributor II

Thanks Edward, your answer partly helped me, but not completely.

in my project, I have a ROM header table allocated in application code, but used in bootloader project for power on flash test.

see below to know the table content:

PRM file:

     SEGMENTS  /* Here all RAM/ROM areas of the device are listed. Used in PLACEMENT below. */

          /* non-paged FLASHs */

           ROM_CS          = READ_ONLY     0x1400 TO   0x1401;     // App code checksum

           ROM_1400       = READ_ONLY     0x1402 TO   0x1FFF;

           ROM_4000       = READ_ONLY     0x4000 TO   0x7FFF;

           ROM_ENTRY      = READ_ONLY     0xC000 TO   0xC06F;

           ROM_VECTORS    = READ_ONLY     0xC070 TO   0xC0FF;

           ROM_C000       = READ_ONLY     0xC100 TO   0xEFFF;

           ROM_F000       = READ_ONLY     0xF000 TO   0xFEFF;    /* Bootloader preserved */

     END

     PLACEMENT

            _PRESTART,              /* Used in HIWARE format: jump to _Startup at the code start */

            STARTUP,                /* startup data structures */

            ROM_VAR,                /* constant variables */

            STRINGS,                /* string literals */

            VIRTUAL_TABLE_SEGMENT,  /* C++ virtual table segment */

            //.ostext,              /* OSEK */

            NON_BANKED,             /* runtime routines which must not be banked */

            COPY                    /* copy down information: how to initialize variables */

                                    /* in case you want to use ROM_4000 here as well, make sure

                                       that all files (incl. library files) are compiled with the

                                       option: -OnB=b */

                              INTO  ROM_1400, ROM_4000;

            DEFAULT_ROM       INTO  ROM_C000, PAGE_08, PAGE_09, PAGE_0A, PAGE_0B, PAGE_0C, PAGE_0C_A000, PAGE_0E;

     END

     CHECKSUM

            CHECKSUM_ENTRY

              METHOD_ADD

              OF   READ_ONLY 0x4000 TO 0x7FFF     /* ROM_4000 */

              OF   READ_ONLY 0xC000 TO 0xEFFF     /* ROM_C000 */

              //OF   READ_ONLY 0x88000 TO 0x8bfff   /* PAGE_08  */

              INTO READ_ONLY 0x1400 SIZE 2

              UNDEFINED 0xff

            END

     END

in Application code, main.c, the ROM header structure is defined as below,

typedef struct SECTION_HEADER_TYPE_TAG{

   //U32 Startup;      /* _Startup entry address, must be in local flash */

   U32 Rom_Begin;    /* ROM beginning address to calculate checksum  */

   U32 Rom_End;      /* ROM end address to calculate checksum  */

   U16 Rom_Cs_Addr;  /* ROM checksum address, local flash */

   struct SECTION_HEADER_TYPE_TAG const* Next_Section_Header;

}SECTION_HEADER_TYPE;

#pragma CONST_SEG APP_ROM_ENTRY

extern char __SEG_START__PRESTART[];

extern char __SEG_END_DEFAULT_ROM[];

#define ROM_SECTION_1400_START     0x1400UL

#define APP_ROM_CS_ADDR            ROM_SECTION_1400_START

const SECTION_HEADER_TYPE App_Section_Header  /*@ROM_SECTION_C000_START*/ =

{

   (U32)__SEG_START__PRESTART,

   (U32)__SEG_END_DEFAULT_ROM,

   APP_ROM_CS_ADDR,

   NULL,

};

in the map file, I can see the address lables generated as below:

- LABELS:

     __SEG_START__PRESTART                     1402       0       0       2              

     __SEG_END_DEFAULT_ROM                     C410       0       0       2              

as you see, I can resolve Rom_Begin, but for Rom_End, I want it at 0xEFFF, as it defined in CHECKSUm, but compiler gives it the dynamic address decided by code size,

also it can't resolve Rom_Cs_Addr, because it's not used in App code,  there is no placement name for it.

3,048件の閲覧回数
kef2
Senior Contributor V

I knew __SEG_xxx won't help you. Unfortunately CW doesn't have means to determine in the code the start and end of particular PRM SEGMENT, only start and end of PLACEMENT, where end depends on the size of placed stuff.

This is also why I'm not using PRM CHECKSUM feature. Looks great until you try to use it for anything else than code checksum. I think that either CHECKSUM should be able to crc from __SEG_START to __SEG_END, or there need to be some other linker defined symbols for start and end of PRM SEGMENT or PRM defined top of PLACEMENT. If you need this feature, then you may like to make service request asking for this feature.

Regards

Edward

0 件の賞賛
返信