HCS08 profiling and analysis

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

HCS08 profiling and analysis

1,367件の閲覧回数
zorrotz
Contributor III

Working with MC9S08SH16 MCU in CW V10.2, I enable trace and profile to collect trace data and then I start program execution. I found that the program does different things if I enable trace and profile or not. During program execution some RAM and CPU register test functions are executed, and when trace and profile is enabled this functions show problems.

Does trace and profile modify MCU RAM content?

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,090件の閲覧回数
carloscuev
Contributor V

How did you enabled Trace and Profile in a HCS08 CPU? I'm working in QB8 and AFAIK there's no support for HCS08

0 件の賞賛
返信