HC12: declaring large data arrays in external memory

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

HC12: declaring large data arrays in external memory

ソリューションへジャンプ
4,341件の閲覧回数
NZ_Design
Contributor I
             BatteryRAM      = NO_INIT       0x200000'G TO 0x3FFFFF'G;  // CS1
             Bat_RAM              INTO  BatteryRAM;
typedef struct
{
 unsigned char cOutExit;
 unsigned         bOutFired:1;
 unsigned char cBatchExit;
 unsigned char cLabelPoint;
 unsigned char cFruitSize;
 unsigned int    iFruitWeight;
}BED;
 
#define MAX_BED              0x03FF
#define MAX_LANES          16
 
#pragma DATA_SEG __GPAGE_SEG Bat_RAM
 char cExt_RAM[56];
 Prog_Layout Program[9];
 BED FruitBed[MAX_LANES][MAX_BED];
#pragma DATA_SEG DEFAULT
L4100: Failed to convert address 0x200000'G of FruitBed because of 'External space area (140000..3FFFFF) has no logical address'

L4100: Failed to convert address 0x200000'G of In debug info because of 'External space area (140000..3FFFFF) has no logical
address'

L4100: Failed to convert address 0x200000'G of In debug info because of 'External space area (140000..3FFFFF) has no logical
address'

That is understandable but how do I declair my arrays so as the complier recognises them.
My old compiler wasn't able to cope with paging so I did it manuallly in my code. Putting each lane on a seperate page at the same address. I are trying to get away from this.
 
Does anybody have a good surgestion.
 
Daniel

Message Edited by CrasyCat on 2007-04-13 01:24 PM

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
2,335件の閲覧回数
CrasyCat
Specialist III
Hello
There seems to be something wrong in the application.
Please submit a SR for that through our on-line support web page and attach the whole project reproducing the trouble.
 
Our support people will be able to look into that and identify the problem.
 
CrasyCat

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
2,335件の閲覧回数
NZ_Design
Contributor I
The processsor I are using is MCS12XDP512 and code worrier version is 5.7.0
 
I re wondering if I should be setting up indervidual pages and assigning the pages to Bat_RAM.
 
Daniel
0 件の賞賛
返信
2,336件の閲覧回数
CrasyCat
Specialist III
Hello
There seems to be something wrong in the application.
Please submit a SR for that through our on-line support web page and attach the whole project reproducing the trouble.
 
Our support people will be able to look into that and identify the problem.
 
CrasyCat
0 件の賞賛
返信
2,335件の閲覧回数
CrasyCat
Specialist III
Hello
 Which CPU are you targeting?
 Which version of CodeWarrior are you using?
 To retrieve that information:
    - Start IDE
    - Select Help -> "About Freescale CodeWarrior"
    - Click on "Installed Products"
    - Click on "Save As", save the result in a file and attach it to that post.
 
CrasyCat
0 件の賞賛
返信
2,335件の閲覧回数
CompilerGuru
NXP Employee
NXP Employee
One reason for this warning is if you do only surround the definition of the variables with a
#pragma DATA_SEG __GPAGE_SEG Bat_RAM
but not the declarations of the variables.
I recommend to always use the same #pragmas before/after both, and to include the header file declaring the variable also in the C file defining the variable so the compiler can issue a warning:
>Warning : C4200: Other segment than
>in previous declaration

in case of a inconsistency.

If the compiler does not know that an external variable should be accessed with __GPAGE_SEG,
and the debug information will refer with logical addresses to it and this does cause this message.

Note also that this is just a warning about the debug information (and not about code).

Daniel
0 件の賞賛
返信