HC08: Targets interfaces

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HC08: Targets interfaces

4,901 Views
Br
Contributor I
Do you know where can I download targets files for HIWAVE program? The file extension is '.tgt'. I´m needing the BDM_HCS08.tgt file.

Thanks

Emerson

Message Edited by CrasyCat on 2007-04-13 11:40 AM

Labels (1)
Tags (1)
0 Kudos
Reply
5 Replies

3,291 Views
Br
Contributor I
Hello Daniel,

I´m looking for this target because it have some FLASH commands that permit to program, erase and verify FLASH contents using the BDM interface. I think that the HCS08FCS.tgt and HCS08ICDCYCLMULT.tgt do not have this commands. I will try it and after this I will put a conclusion here.

Thanks for your attention

Emerson
0 Kudos
Reply

3,291 Views
CrasyCat
Specialist III
Hello
 
Please refer to Expert Mode Programming in the HC08 Debugger manual for information on Flash programming commands.
 
CrasyCat
0 Kudos
Reply

3,291 Views
Br
Contributor I
Hello,

I did it, but I do not have the BDM_HCS08.tgt file to be selected. The targets that appears are:
HCS08FCS.tgt
HCS08ICDCYCLMULT.tgt
HCS08SERIALMON.tgt
SOFTEC_HCS08.tgt

And I want this target file : BDM_HCS08.tgt

Do you know how i can get this file?

Thanks

Emerson
0 Kudos
Reply

3,291 Views
CompilerGuru
NXP Employee
NXP Employee
Sorry, I don't have it for you :smileysad:.

But anyway, why do you need exactly this BDM_HCS08.tgt?
AFAIK, this is the name of the old target connection to the P&E driver. It has been replaced by the HCS08FCS.tgt (simulation) & HCS08ICDCYCLMULT.tgt (hardware) targets.
So do they not work for you?

Well, I'm not the expert in those connection setups, but to my understanding, they should provide all the functionality the BDM_HCS08.tgt did use to provide.

I think the last version which did contain this target interface was the HC08 V3.1.

Daniel
0 Kudos
Reply

3,291 Views
CrasyCat
Specialist III
Hello
You can load a connection selecting  "Component" -> "Set Connection".
The Set Connection dialog should display all available connections.
 
CrasyCat
0 Kudos
Reply