GNU & CW10 on same PC?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

GNU & CW10 on same PC?

1,404 Views
dougpaulsen
Contributor IV

Can the Eclipse based GNU development system and the Eclipsed based CW10 both co-exist on the same PC?

 

After a arduous process, I have the Eclipse IDE for C/C++ Mars.1 Release 4.5.1 installed and operational on my main PC.  My next development will require Codewarrior 10.  It would be most desirable to have both applications on one PC, but I understand Codewarrior 10 is ALSO Eclipse based.  Will there be a conflict between the two installs?  Obviously, I don't want to break one by installing the other.... 

 

Thanks for any comments, warnings, or advice in general!

#codewarrior 10

#GNU

#GCC

compatibility

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

1,280 Views
BlackNight
NXP Employee
NXP Employee

I have multiple Eclipse IDE's and GNU toolchains installed on my machine, and not faced any issues that way with CodeWarrior, as it is using the toolchain inside the CW inststallation.

Erich

0 Kudos
Reply