Full Chip simulator problem for MCF51JE256

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Full Chip simulator problem for MCF51JE256

1,438件の閲覧回数
gustavod
Contributor III

Hi,

 

I'm using CodeWarrior 6.3 with MCF51JE256 microcontroller.

I'm able to compile my project, but when i try to do the full chip simulator there is no JE microcontroller into derivatives options.

 

Is there a workaround for that?

 

Best regards,

Gustavo

ラベル(1)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,283件の閲覧回数
kef
Specialist I

Do you have JE256 service pack installed? CW 6.3. updates:

http://www.freescale.com/webapp/sps/site/overview.jsp?code=CW_UPDATES_MCU_63

0 件の賞賛
返信

1,283件の閲覧回数
gustavod
Contributor III

Yes. The service pack allows to compile the code, providing include files and libraries for JE256. Without this service pack is impossible to compile code for JE256/128.

 

However, apparently full chip simulator is not supported.

0 件の賞賛
返信